(0)| 2/19/2019 9:33 AM | |
|
Posts: 2 Rating:
|
Dear Sir/Madam, I have one issue to address here and request your support to resolved the issue. In one of my motor feeder we have Simocode pro C using for motor protection and controlling the motor and simocode Pro C has connected with profibus DP to DCS for the communication, the main problem is that whenever motor get tripped by overload or rotor stall fault we acknowledge the fault by pressing reset button on simocode .However, when the motor tripped by same fault for than one to two time , the bus indication is not getting healthy but after 3 to 6 hours waiting then bus indication getting healthy . what could be the possible reason ?? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 2/20/2019 10:46:45 AMNew subject after splitting |
|
Follow us on