(0)| 3/16/2019 2:11 PM | |
|
Posts: 9 Rating:
|
Dear Sir Hi, Thanks for your information. I have some questions in regard of cement batching plant if you can help us. For weighting system we use 4 load cell transducers with Modbus RTU output to connect them to s7-1200. Is it possible? I mean is it accurate and fast enough for reading weight? For aggregate gates we use pneumatic air cylinder to open or close them? i wanted to know is that all that we have to do to control the weight? to have an approximate weight with max 10 kg error? or should we design a PID loop in PLC to close the gate? Thanks in advance for your time ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/18/2019 7:42:21 AMNew subject after splitting |
|
| 3/18/2019 7:47 AM | |
|
Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject Questions regarding cement batching plant is published within the conference Process Instrumentation / Analytics / Weighing Systems SIWAREX. Best regards Jen_Moderator |
Follow us on