(0)| 10/6/2008 10:01 AM | |
|
Posts: 1611 Rating:
|
....Is there an easy way to log alarms on a network pc, panel is MP377 connected on the network. What settings should I make..... --> That is no problem. Read this FAQs -> http://support.automation.siemens.com/WW/view/en/13336639 -> http://support.automation.siemens.com/WW/view/en/26190516 ....Is a combination of the two possible : continiusly logging on the MMC and logging on the network at the same thime..... --> You can do this, but for what? You use two archive, one with the path \\Network\... The other one with the path \Storage Card MMC\.... ....Is it also possible to transfer the loggs at certain periods to a pc on the network, every transfer is written to a different file with only the new data... -> Read this FAQ -> http://support.automation.siemens.com/WW/view/en/28937151 Sorry, that i give you so many FAQs, but i think they could be helpful for you. |
Last edited by: The Brain at: 10/6/2008 10:01 AM |
|
Follow us on