(0)| 4/26/2019 8:03 AM | |
|
Joined: 5/3/2017 Last visit: 12/5/2025 Posts: 673 Rating:
|
Hello woffkin, Maybe the error occurs, because the OS Runtime was activated once unintentionally on the ES (not simulating OS RT). Consequently the databases (OS(1)ALG.ldf or OS(1)ALG.mdf, for example) were created on the ES. With the subsequent download these database files that are on the server are supposed to be overwritten. However, the files on the server are "occupied" by the SQL server. This then can lead to the download being aborted with an error message. If so, Siemens offers in the FAQ What should you do if the OS server project is taken online by mistake on the ES? a workaround to solve the problem. With regards |
This contribution was helpful to
|
|
Follow us on