(0)| 4/12/2006 11:11 AM | |
|
Posts: 1084 Rating:
|
Hi, If i remember correctly, the migrator needs also sybase 7. In version 5.1 wincc used sybase 7 instead of sql server as which is used in wincc 6.x You need to install sybase 7 as well on your system to be able to migrate your project. The following Text is substracted out of the .chm help file that can be obtained from this FAQ entry: http://support.automation.siemens.com/WW/view/en/19219424 Sybase SQL Anywhere 7 can be installed later using the Autorun program on the WinCC V6.0 CD. To do this, the installations CD for WinCC V5.0 Service Pack 2 or WinCC V5.1 is required. with regards, Ikkezelf |
Last edited by: Ikkezelf at: 4/12/2006 11:20 AM |
|
Follow us on