(0)| 5/16/2019 11:34 AM | |
|
Joined: 10/1/2018 Last visit: 10/28/2025 Posts: 74 Rating:
|
My software (TIA Portal) doesn't detect the ET200 module. It displays the following message when I check the diagnosis status: 'No diagnostics data available because the current online configuration data differs from the offline configuration data'. I have double checked the modules configuration in TIA Portal and they are the same as the hardware ones. The light BF of ET200 is red and the light SF of PM is red too. Could you tell me what is the problem and how can I solve this? Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/16/2019 14:48:02New subject after splitting |
|
| 6/24/2019 12:15 PM | |
|
Joined: 8/21/2014 Last visit: 12/19/2025 Posts: 1098 Rating:
|
Closed, because the same question is also posted here:SF light of the PM module is ON and the BF light of ET200 is ON |
Last edited by: Jen_Moderator at: 07/09/2019 10:55:23Inserted link from thread. My Forum is the place to personalize your profile, |
|
Follow us on