(0)| 6/27/2019 7:13 AM | |
|
Joined: 3/14/2008 Last visit: 12/28/2025 Posts: 2233 Rating:
|
Hi HarrY, The only way I can think of now is by checking the instance datablock of the two motor blocks in CFC and then open the "Blocks" folder where you open one of the instance datablocks and enter online view. Then go to Datablock and select Open where you select the next instance db. Then you put them next to each other so you can compare differences.... |
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on