(1)| 7/8/2019 9:30 AM | |
|
Posts: 226 Rating:
|
Hello what are the risks of integrating a third-party controller in a Desigo Insight or Desigo CC environment ?? Wago Bacnet/ip |
| 7/8/2019 6:11 PM | |
|
Joined: 11/8/2017 Last visit: 12/16/2025 Posts: 360 Rating:
|
Hi, Apart from the usual networking / IT security considerations, integrating this device directly into either Desigo CC or Desigo Insight should not be an issue. CC has a good method for auto-discovery of 3rd party devices and points. The process to integrate to CC is fairly straight forward. Desigo Insight is similar, but different. The PICS statement is attached for the Wago device. The only issues you may run into would relate to the 3rd party device BACnet conformance - i.e. something doesn't work quite as it should (i.e. a Schedule can be Read into CC - but can not be Written to from CC). Some devices will be perfect, some will have issues though. Regards, AttachmentPICS_t07500831_xxxxxxxx_0en.pdf (641 Downloads) |
This contribution was helpful to
|
|
Follow us on