7/23/2019 6:48 AM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (77) |
Hi all, HMI- Assembled PC with Windows 10. RT Advanced- 6AV21040BA050AA0 Software- TIA V15 Issue- The HMI software is developed in V15 but there is V15.1 on actual PC. Strangely same versions for confi. & runtime are available on actual site PC also. When program is put into runtime, it returns with popup message of incompatibility. Pl see attached snaps. What is shortest way to resolve the issue ? Also share link for only WInCC V15.1 confi. advanced. AttachmentNew folder.zip (26 Downloads) |
Last edited by: Sachinpatke at: 07/24/2019 06:00:29If you like the comment, rate it (right top) or thank it (left bottom). |
|
Follow us on