10/14/2008 1:00 PM | |
Posts: 3 Rating:
|
1. We installed and configured the SImatic OPC server and OPC client (Scout) on the same machine. The connection was ok. OPC scout could able to read the value. Attachmenterror.zip (837 Downloads) |
This contribution was helpful to
1 thankful Users |
10/30/2008 1:13 PM | |
Posts: 5822 Rating:
|
Hello, well, if you follow all the steps shown in the OPC White paper by the OPC Foundation it should run. Using OPC via DCOM with XP SP2 v1.10.pdf A detailed diagnostics will not be really successfully over a forum, you need to be right in front of the system to know more. Well, maybe on thing you may check also: Grant the user access to the remote server. Run DCOMCNFG and Select theSIMATIC NETOPC Server Application Properties. Select the Identity tab, and select the interactive user, (by default the launching user is selected and this prevents the remote connection). Maybe this helps. Best regards J_Bell |
This contribution was helpful to
1 thankful Users |
Follow us on