11/8/2019 9:03 PM | |
Posts: 3 Rating:
|
Hi, I am getting stuck on programming a logo 8. For a project i am controlling a pto at a maximum rpm. i want to close a valve at a maximum of 2800 rpm and when it drops down to 2200rpm i want to open it again. the sensor at the fast input of the logo gives 8 pulses each rotation of the pto. also i want to show the rpm on the logo display. i tried to use some of the examples given on this forum but i get stuck on the mathematical settings on some blocks. can someone with more experience help me out and give me a kick in the right direction? regards ls AttachmentSpeed.zip (316 Downloads) |
11/10/2019 9:24 PM | |
Posts: 3 Rating:
|
aah somthing went wrong with zipping the file, my apologies. The program in this zip file i used as a base for the rpm part in my program, i found it on this forum (thanks for that). My total program is a network of 6 plc's i dont now if i use a setting of 18000 in block b004 (calculation of speed) is accurat for my type of sensingi AttachmentSpeed.zip (326 Downloads) |
11/10/2019 10:15 PM | |
Posts: 3 Rating:
|
thank you for your reply. but my input sensor gives 8 signals a rotation so it must be times 8 i think? |
Follow us on