(0)| 11/21/2019 12:13 PM | |
|
Posts: 4 Rating:
|
Hello I got in trouble with communicating a MasterDrives MC (6SE7021-0EP50-Z) unit version 1.6. Tried to connect by 'Based on factory setting', 'Empty parameter set' and didn't found in USS Online connection. Also increased Task timeout value to 20s. BUS type was USS, Interface was COM1, Baudrate was 9600, BUS operation was Automatic, Request retries 100 and respond timeout 40. In my laptop, I have DriveMonitor V5.04.02. I have tried with a RS232 cable which i tested by communicating with other drives (Simovert VC) and found working fine and this make sure that I have no issue with laptop COM port. In drive, parameter settings are: P060=7 P053=6 P701.1=6 P702.1=127 P703.1=2 How could I get out of the problem? Pls suggest me. TIA. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/22/2019 07:31:36New subject after splitting |
|
Follow us on