(0)| 11/14/2019 10:23 AM | |
|
Posts: 12 Rating:
|
Hey, I have data log created in S7-1500, now I have to make it stored automatically on the operator PC (PC and PLC are in the same network). Manually downloading data log is simple - I log in to web server, download log. However, I need it to be made automatically. I found very similar problem here: Given answer was to write a VBA code downloading Data logs from web server. Still, I'm not sure how I could make it execute. As it was mentioned in topic above, copying direct link to download results in 'access denied' error on web page. Other idea I have is to create custom web page with stored data logs, but problem is the same - how to make executable program downloading it on it's own? Any clues / tips apprectiated. Thanks! |
Last edited by: Gostenn at: 11/14/2019 10:39:49 |
|
Follow us on