12/21/2019 7:47 AM | |
Joined: 1/22/2014 Last visit: 9/18/2024 Posts: 32 Rating: (0) |
Hello, I have read this topic and have the same question, I do not fnd the answer. We want to have/send a bit to the PLC when someone is connected with SmartClient to the Smartserver of the HMI. I saw that there are also HMI Option+ tools. But is there something (Area Pointer?) that we can use to signal to a CPU when another person is remotely connected and use the HMI ? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Perreke at: 12/21/2019 07:48:39Last edited by: Jen_Moderator at: 12/23/2019 07:38:04New subject after splitting |
|
Follow us on