(0)| 11/17/2008 11:33 AM | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Posts: 8 Rating:
|
Hi Dear sirs/madams I want to select a redundant S7-414H for a PMS(Power Managament System) My I/O Counting is : 1256 :DI 448 :DO 163 :AI ET200M: 9 But I have just seen a catalog of siemens with strange information: this Link: https://www2.sea.siemens.com/Products/Process-Automation/Product/SIMATIC+PCS+7/Automation+System+Hardware+Controller/Automation+System+Hardware_Controller.htm contains: (
Note The values listed here are not maximum AS-specific values for their respective model, they represent one typical distribution of the totally available for a representative mixture of I/O. Individual calculation of system capacity and performance is possible for actual systems using the configurator software present on the current CD-ROM of the interactive catalog CA 01. if really these are true , I cant use oneS7-417H too they differs too much with max. Number of I/Os in Catalogs Do you think My System can be done by 414H? |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| 11/17/2008 3:26 PM | |
|
Posts: 125 Rating:
|
Hi, A maximum of total I/O address area is 8KB = 65536. See system manual chapter 17, Address areas(inputs/outputs) http://support.automation.siemens.com/WW/view/en/1186523 |
| 11/19/2008 4:01 PM | |
|
Posts: 3149 Rating:
|
Hi perhaps these FAQ can give some additional information http://support.automation.siemens.com/WW/view/en/17294496 http://support.automation.siemens.com/WW/view/en/16771059 http://support.automation.siemens.com/WW/view/en/16923947 Anyway I would recommend as Danielle said to contact your local PCS7-promotor nemo |
Follow us on