(0)| 11/17/2008 6:36 AM | |
|
Posts: 2348 Rating:
|
what type of connection do you create? |
| 11/20/2008 4:12 AM | |
|
Posts: 9 Rating:
|
I havechecked the number of connections in use during communication and yes there is 4 S7 connections for CPU315.Out of these4, 2 connections have been usedup for redundant connection to CPU417.2 connections remained available. However, the number of connections seemed to be independant of the number of links in use. The link mentioneduses communication blocks FB14 "GET" and FB15 "PUT" for data communication between CPU315 and CPU417. Referring to the attached manual, it is referred as R_ID. I need to know how many R_ID (pairs of GET and PUT communication blocks) can I configure whenI use CP343-1 lean, CP343-1 full and CP343-1 Advanced version, if that matters. I need 10 links. Will appreciate any suggestions. AttachmentSFC_e.pdf (333 Downloads) |
| 11/21/2008 3:09 AM | |
|
Posts: 9 Rating:
|
Thanks, J_Bell. Is there a manual that gives the techincal information on how many links I can configure with various type of CP ? |
| 11/21/2008 11:41 AM | |
|
Posts: 5822 Rating:
|
Dear Yen, well, there are a lot of samples. Maybe one of these will help. What differences are there when configuring S7 connections? What should you watch out for when configuring an unspecified S7 connection for data communication between an S7-300 and an S7-400? How do you configure an S7 connection for data communication between an S7-200 and an S7-300 or an S7-400 at the Industrial Ethernet? Best regards J_Bell |
Follow us on