(0)| 11/14/2007 4:30 AM | |
|
Posts: 18 Rating:
|
Dear All, Also when we see the installed software, we could see all the required software installaed with correct version. We just want to know what is the meaning of these errors & how they would affect the software development. The file attached herwith is in ZIP format because of memory constraint. AttachmentPCS7 V7 Sp1 error.zip (260 Downloads) |
| 11/14/2007 6:58 AM | |
|
Joined: 5/19/2006 Last visit: 1/11/2026 Posts: 550 Rating:
|
I suspect you might run out of PATH size (I believe 1024/2048 char for XP sp1/sp2). |
Last edited by: Dec at: 14.11.2007 07:17 |
|
| 11/14/2007 10:04 AM | |
|
Posts: 18 Rating:
|
Dear Dec, I have checked the path length & same is attached here for your reference. As per you information it is reaching to only 1007 with no spaces & 1041 with spaces.Since both pcs having Windows XP SP2 installation. So the length shoult not be a problem. Also referering to previous thread, errors regrading path could not be copied for SFC visualisation & version cross checker during installation, but the same path name is existing in CONTROL PANEL>SYSTEM>ADVANCE>ENVIRONMENT VARIABLE>SYSTEM VARIABLES>PATH& same can be verified in pathentry file attached herewith. Thanking u in advance Bheja AttachmentpATH ENTRY.zip (217 Downloads) |
| 12/1/2008 11:40 AM | |
|
Posts: 993 Rating:
|
Hello Bheja, did you solve your problem or does it actually occurs? Cumu |
Follow us on