(3)| 4/2/2020 12:54 PM | |
|
Posts: 3 Rating:
|
Dear All, I have an issue, with erasing DB. Problem following: 1. Before erase DB, I use ANY pointer format in FC and read quantity of bytes into attached to fc DB. 2. I write 0 to each byte Whenever type of value in DB Real/Int/Bool/Word/Dword… it is work fine, but if it is string type or Wstring, then I can not overwrite first byte, due to problem with sizing string value. So, Is it possible to via opening DB, like OPN[DB_Number] found, which byte correspondent to which data type valye? Thanks for helping ------------------------------------------------------------------------------------------ |
Last edited by: uakivso at: 04/02/2020 12:55:15Last edited by: Jen_Moderator at: 04/02/2020 13:24:40New subject after splitting |
|
| 4/3/2020 7:55 AM | |
|
Posts: 623 Rating:
|
Hi, May be possible for S71200/1500 using variants in TIA. |
This contribution was helpful to
|
|
| 4/7/2020 2:23 PM | |
|
Posts: 3 Rating:
|
OK, clear. Thanks a lot |
Follow us on