(0)| 12/5/2008 6:05 PM | |
|
Posts: 95 Rating:
|
Hi I am using an MP370 with a S7-300 PLC. I have enabled several datta logs. I am using Sm@rtService to download the archive files for import to Excell. The archive is a real data point. When you import the data you can select the delimiter. If you select comma, it destroys the real data because it uses a comma instead of a period. Any ideas around this? thanks John |
| 12/17/2008 4:47 PM | |
|
Posts: 95 Rating:
|
Zak Thanks! that worked. Just note that you have to delete the archive file for the change to work. I did that by loging into the HMI (I am connected to this using sm@rtservice over the internet), and then I started the task bar. From there I was able to start the file browser and use Windows functions to delete the file. John |
Follow us on