(0)| 6/1/2020 11:45 PM | |
|
Joined: 3/14/2008 Last visit: 12/28/2025 Posts: 2233 Rating:
|
Hi, This would be an excellent case for block TimeTrig (FB1802) from the APL library. The block allows daily, weekly or monthly generation of a trigger. Connect the output trigger of the TimeTrig block to the .In variable of a CountScl (FB1806) The block will count up or down each time a trigger is given. Make sure you set .LiOp and .UpLi both to "1" so the counter is incremented by software logic rather than operator. |
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on