(1)| 5/20/2020 12:26 PM | |
|
Joined: 3/14/2008 Last visit: 12/28/2025 Posts: 2233 Rating:
|
Yes, That is correct, driver blocks are the connection between hardware and software. They do not feature block icons since they only read out values and determine the quality. Also necessary connections are made so that the actual value source is retrieved like 4-20mA signal or 0-10mV. You can connect the driver block values to the corresponding APL blocks you described. |
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on