(0)| 6/17/2020 4:50 PM | |
|
Posts: 137 Rating:
|
Hi all. I have configured MCP 438 in OB100. I have ncu730 3 pn. My problem is that on MCP all the outputs led are random i.e when I press X button a LED for a user-defined button will lit up. The same goes for a lot of buttons. What could be the cause of the issue? ? ...sent from App I also get an error on the HMI 1) Emergency stop (error code 3000) and 2) Fault on PROFINET bus. I hade this fault earlier and the MCP was continuously blinking the LEDs but then it stops and now I have the same error code with new problem explained above. AttachmentOB100 Config.zip (170 Downloads) |
Last edited by: Divej93 at: 06/17/2020 16:57:02 |
|
Follow us on