(1)| 12/26/2008 8:54 AM | |
|
Joined: 10/31/2005 Last visit: 4/22/2025 Posts: 366 Rating:
|
Hello to all, I'm having very same problem: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=24456113&caller=view Now, I need your help. I need to download whole wincc flex project again in order to restore password. I have a good working knowledge about STEP7, butnever worked with WinCC Flexible 2005. I need step by step guide. I have PG with WinCCflex project. OP TP170B color panel is connected to the CPU 314via profibus cable to MPI port. Connector on CPU 314 (inserted into MPI slot) has a porton itself which is used to connect PGto modify program. ON OP panel there are two more ports (RS232 which are not used) 1. Should I connect my PG toport on connector that is inserted into MPI port on CPU314? 2. Is there any way I can turn off option to disable password when enetered three times wrong? 3. When connected, after I open wincc flex project, how to perform download to OP panel? How to check connection to OP panel? Additional questions: 4. In transfer settings I guess I'll need to check Overwrite password list, right? 5. Can this action disturb online process in any way? Thanks in advance |
Last edited by: Pandiani at: 12/26/2008 8:59 AM |
|
Follow us on