(0)| 7/9/2020 4:04 AM | |
|
Posts: 3 Rating:
|
HI Bergmanu ! I'm doing project using IoT2020 with S7-1200 (article no: 6ES7 212-1AE31-0XB0). The problem with the PLC im using right now does not have enable the permit access with put/get communication as stated in tutorial (as in pic attached); My question are, can i proceed my project without follow the step of enabling permit access put/get? if i can proceed, is there any additional line of ladder to put inside the Program Block? I'm very new with PLC and still learning. Hopefully, my project will done successfully. Thank You ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/09/2020 06:29:15New subject after splitting Last edited by: Jen_Moderator at: 07/09/2020 08:21:44Optimized headline. |
|
| 7/9/2020 11:09 AM | |
|
Posts: 3 Rating:
|
Thank you for the info bergmanu. If that so, i will proceed to use the plc. |
Follow us on