(0)| 7/21/2020 3:02 PM | |
|
Joined: 9/9/2014 Last visit: 2/12/2025 Posts: 246 Rating:
|
Hello! first of all: Read the manual below SIMATIC ET 200MP digital I/O module F-DI 16x24VDC Next: All the connection diagrams that you need are indicated in the points 5.3Application 2: Safety mode SIL3/Cat.3/PLe Page 37 Digital input module F-DI 16x24VDC (6ES7526-1BH00-0AB0) Manual, 01/2016,A5E03858068-AA Ok, next again)) An example of connection from the manual is attached. For emergency buttons, normally closed one or two contacts are always (usually) used (depending on requirements) I would on my own - recommend using a connection with an external power source - L + But this is just a matter of preference))) |
|
Best Regards |
|
Follow us on