(0)| 9/14/2020 4:01 PM | |
|
Joined: 6/30/2006 Last visit: 1/13/2026 Posts: 1 Rating:
|
Hi, I have same problem. Siwarex FTA is not responding after Firmware update. There is some communication between Siwatool <-> FTA , because when trying to go online with Siwatool it says that 'The connected module cannot be accessed by this application.' and when i remove the cable it only tries to get connection. This is with Set/reset download mode selected and Siwarex powered on with switch in lower position. I have tried Siwatool 2.3.5 and V4. Any suggestions? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 09/21/2020 12:00:20New subject after splitting |
|
Follow us on