(0)| 10/26/2020 10:28 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello Vicius; A long time ago I remember the SLC 5/04 would work with Modbus RTU. Does your SLC 5/03 provide the same interface? If so, adding a CM PTP module on the ET 200SP rack would allow serial comms between the 2 processors, one acting as master, the other as slave.Here is an application example for the ET 200SP: Master-Slave Communication via a CM PtP using the Modbus RTU Protocol https://support.industry.siemens.com/cs/ww/en/view/68202723 Hope this helps, Daniel Chartier |
Follow us on