(2)| 11/20/2020 2:39 PM | |
|
Posts: 198 Rating:
|
Hello Berg, Although there is no separate block to achieve the I-PD or PI-D configuration with APL Library, it is possible to achieve 'switching of P or D action into the feedback path' in the PidConL block. For achieving this, -> Set PropFacSP = 0:Proportional action is completely in the feedback path (with this setting) -> Set DifftoFbk = 1:Derivative action is in the feedback path. Setpoint jumps do not affect the derivative action.(with this setting) ---- More information on this configuration, refer 'Structure Segmentation at Controllers' section in the Advanced Process Library Manual ---- Please rate my answer if it was useful to you :) |
Last edited by: TechnoBlaze at: 11/20/2020 14:41:54Last edited by: TechnoBlaze at: 11/20/2020 14:42:52Last edited by: Jen_Moderator at: 11/23/2020 08:25:17Optimized link. |
|
This contribution was helpful to
|
|
Follow us on