12/16/2020 1:26 PM | |
Posts: 5 Rating: (0) |
hello, Nikzitronik I have a project also with V16 pro and IS, after many tests I managed to make the two communicate, Wincc Server and IS Server both equipped with win server 2012 r2. in IS I can point out the Wincc project and see the tags however I can't access the stored values. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/17/2020 07:59:48New subject after splitting |
|
Follow us on