(0)| 1/10/2021 3:52 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello Tidelec; The short answer is provided by our friend Hulzhex in the following discussion: - CP342-5 Profibus Master with Slave DPV1 will that work A bit more information can be found in the manual and technical data of the CP 342-5: - SIMATIC NET: S7-300 - PROFIBUS CP 342-5 / CP 342-5 FO - Manual Part B https://support.industry.siemens.com/cs/ww/en/view/8773570 The CP 342-5 can only work as a Profibus DPV0 master (or slave). If it connects to a slave DPV1, the slave DPV1 functions cannot be activated, and it must limit itself to cyclic exchanges, with a maximum of 244 bytes of parameter data. The IM 55-6 DP HF manual explains why you get this error message with a DPV0 master, see the screenshot below. https://support.industry.siemens.com/cs/ww/en/view/73098660/112801182731 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 01/10/2021 15:52:52Last edited by: dchartier at: 01/10/2021 17:37:38 |
|
Follow us on