(0)| 1/17/2021 2:04 PM | |
|
Posts: 4 Rating:
|
Hello, We are having the same problem 043 PLC-CPU not ready for operation. Checked PLC service display and found the fault was for 6F F0000 4000 3000 2000 1000 which is for IO startup error Checked the power supply, no blown fuse There was no lights on the remote backplane, replaced it and now we have amber and red light Replaced the IO modules, still the same issue Reseated the interface cables on the MCP Now we have 2A F0000 0000 0000 0000. Which I believe is for data loss. Tried loading the tea2 files from disk and did a general reset but the fault won't go away. I might not be following the right procedure to load the data from disk. Can someone help troubleshooting these issues? Thanks! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/18/2021 12:24:12New subject after splitting |
|
| 1/18/2021 12:25 PM | |
|
Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject 043 ORD1 PLC CPU not ready for operation (6F/2A F000) is published within the conference SINUMERIK CNC automation systems. Jen_Moderator |
Follow us on