(3)| 1/17/2021 9:20 AM | |
|
Posts: 26 Rating:
|
Hello, Can I integrate a BCE communication card into an HP Ordinary PC? Thankyou, |
| 1/18/2021 9:29 AM | |
|
Posts: 26 Rating:
|
Hello, Can I use ordinary ethernet card for communication with PLCs ? Thank you |
| 1/19/2021 1:58 AM | |
|
Joined: 9/9/2015 Last visit: 12/5/2025 Posts: 732 Rating:
|
Hi, Yes, you can. If you do not require redundant communication to S7-400H, then standard BCE is okay. 1. BCE is for AS Single station up to 8. 2. CP 1623/1628 is for communication on AS single station/ redundant AS up to 64 AS single stations. 3. For Plant Bus Communication For more information on the benefit, download this catalogue and search CP 1623. |
|
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to
|
|
Follow us on