(2)| 1/27/2021 7:20 AM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Hi, The big difference is that INT commands are evaluated in Auto and Manual mode, regardless if the modes are enabled (ENRESUME, ENHOLD). Normally you use them inside steps like when a delay time has passed in the SFC, the next step would be INTHOLD to set the SFC to Holding-Held. PS: The commands HOLD, RESUME, ABORT etc. are only valid in Auto mode of the SFC.
|
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
|
|
Follow us on