(4)| 1/26/2021 4:38 PM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Hi, Do you mean this:Link |
Last edited by: Oreca at: 01/26/2021 16:39:49If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
|
|
| 1/26/2021 6:19 PM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Hi, You need to add the script listed in the link. In the script, you can assign the user and password. Below is a sample from the code:
|
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
|
|
| 1/27/2021 1:18 PM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Hi, Well, you definitely need to define the users and groups in Windows. When logging into SIMATIC Logon, SL will query is the user is know in Windows. After validation, the user is authenticated and then the rights are checked. The information is sent back to SL and in WinCC the configured roles/rights are checked. The script is needed for instance when runtime starts so that the default user can be logged in automatically. |
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
|
|
Follow us on