(0)| 1/27/2021 4:01 PM | |
|
Joined: 9/1/2017 Last visit: 11/19/2025 Posts: 156 Rating:
|
Hi Sorry for writing new post in old topics,but i think it's better that same information stacked up in one place. I had the same situation with 414-4h H station, so can not download to plcsim for time stamp correcton.upgrading pcs7 v7.1sp2 to v8.0sp2 did not solve the problem. At last i exchanged flash memories with the ram memories of another project.( because of operational priority i must startup thevother station and so could n't use ram for time stamp correction ). Two stations have been working fine till now, but is n't there any untricky solution for this issue? Regards hosein ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/28/2021 05:51:19New subject after splitting |
|
| 1/28/2021 11:25 AM | |
|
Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject S7-400H-Flash memory-CFC-Test mode, can not watch online block i/o values is published within the conference Process Control Systems SIMATIC PCS 7. Jen_Moderator |
This contribution was helpful to
|
|
Follow us on