(1)| 2/16/2021 8:51 AM | |
|
Posts: 198 Rating:
|
Hello Kromzie, PCS7 V9.0 is compatible with the following Operating systems (Reference: PCS7 V9.0 Online Readme) ● Windows 7 Professional SP1 (64-Bit, only English Windows language version) ● Windows 7 Ultimate / Enterprise SP1 (32-Bit) ● Windows 7 Ultimate / Enterprise SP1 (64-Bit) ● Windows 10 Enterprise 2015 LTSB (64-Bit) ● Windows Server 2012 R2 Standard Edition (64-Bit) (as "Windows Server 2012 R2 Standard with Update" or incl. KB 2919355 „Windows Server 2012 R2 Update“) Even the latest release, PCS7 V9.0 SP3 is compatible with Server 2016 and not 2019.
OS Server redundancy license is version specific. The OSRTPO license is a count relevant license and the options are available for 100, 1000 and 5000 POs. . The PCS7 licenses are either count relevant or version specific (there is no compatibility of licenses with specific operating systems. The product version - V9.0 compatibility with operating systems matters for the version specific licenses) For more information on licenses, you can refer thePCS7 V9.0 Licenses and Configuration Limits Manual
You may want to checkout the 'Configurator' tab in this link - https://mall.industry.siemens.com/mall/en/WW/Catalog/Products/5109999 -> Select the relevant IPC and click 'Start'. Hope this helps! If you found it helpful, please use the 'Rate' button! :) |
Last edited by: Jen_Moderator at: 02/16/2021 12:58:07Optimized link. |
|
| 2/16/2021 11:45 AM | |
|
Posts: 198 Rating:
|
You can use any count of RT PO as long as you have the appropriate version specific OS Redundancy license along with it. |
Follow us on