(3)| 2/17/2021 12:28 PM | |
|
Joined: 5/3/2017 Last visit: 12/5/2025 Posts: 673 Rating:
|
Hello DPCS, the PCS 7 Industry Library can be download under the following link: If you only want to show the operating hour and you can use the block CountOh. The block CountOh is a standard block from the APL. You only have to connect the Start output from the MotL with the In input of the CountOh block and set the LiOp=1 & UpLi=1. And connect any output from CountOh with the input SelFp1 of the MotL block. With regards |
This contribution was helpful to
|
|
| 2/17/2021 7:22 PM | |
|
Joined: 12/16/2018 Last visit: 1/5/2026 Posts: 75 Rating:
|
Dear Heisenberg2 Your tips and explanations were very helpful and instructive, thank you very much. Best regard |
Follow us on