(0)| 2/10/2021 12:11 PM | |
|
Posts: 1 Rating:
|
dears, We have 2 FIDAMAT 6 to measure hydrocarbon in water. Display showing warming Up and combustible air is not ok. The PLC hold the reading on 18 ppm as last reading received from the analyzer. The DCS has freeze reading also 18 ppm. Analyzer parameters is ok. Combustion air is 485 hPa and hydrogen is 995 hPa and flam-on. What could cause such freezing analysis? Regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/11/2021 08:29:19New subject after splitting |
|
Follow us on