(1)| 2/23/2021 2:41 PM | |
|
Posts: 198 Rating:
|
Hello, In order to configure/enable the diagnostic capability in the multi project (in engineering station), Maintenance ES license is required. Maintenance RT is required on the OS Server or Single station. This is in addition to the PDM license if you are looking at enabling a PDM Maintenance Station Server. Maintenance ES is the base based on which the options to enable diagnostic screens and configure PDM as well. For more information on the license requirements, you can refer the licensing and configuration limits for PCS7 V8.2 . For information on the differences between a Maintenance Basic and Maintenance Standard license, the features are explained in the Maintenance station Manual. Hope this helps! |
Last edited by: Jen_Moderator at: 02/24/2021 07:48:48Optimized links. |
|
This contribution was helpful to
|
|
Follow us on