(0)| 3/3/2021 4:02 AM | |
|
Joined: 5/9/2016 Last visit: 12/27/2025 Posts: 8 Rating:
|
Hi all, can I join the conversation with a different question? We have PCS7v8.1 installed and running with IPC Stations 847D & 547E. We are going to upgrade the system with the latest PCS7v9 without replacing the IPC stations, is it possible to have/buy only a software package to be installed in our existing IPC stations? I would think we buy a recovery DVD for our IPC type and the license of course. Somehow, it's quite difficult to buy Windows OS that supports PCS7v9 lately. We would love to have Win10Pro LTSB but not available on the market now, even for WinServer2016. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/03/2021 09:54:46New subject after splitting |
|
| 3/3/2021 2:08 PM | |
|
Posts: 198 Rating:
|
Hello Nash,
Your two existing IPCs, 847D & 547E will support the PCS7 V9.0 SP3 version. It is possible to buy the software separately. However, stay updated about the upgradation procedures and relevant licenses to be procured.
Please note that IPC847D will support only the following operating systems with PCS7 9.0 SP3:
However, IPC 547E will support only the following operating systems with PCS7 9.0 SP3:
For more information, you may refer the PCS7 V9.0 SP3 Readme file. Hope this helps! :) |
Last edited by: Jen_Moderator at: 03/04/2021 06:36:29Optimized link. |
|
Follow us on