(0)| 3/8/2021 12:15 AM | |
|
Joined: 9/1/2017 Last visit: 11/19/2025 Posts: 156 Rating:
|
Hi There are different blocks and libraries to communicate two AS together like put/get, usend/urcv, bsend/brcv,... Also links for bsend/brcv: Configuring the "BSEND/BRCV" blocks And What should you watch out for when using the blocks BSEND and BRCV in the PCS 7 environment? In pcs7 libraries v7.x and 6.x,there were also two function sets send_r/rec_r and SEND_BO/REC_BO (exchange up to128 boolian type data),which have utilized bsend/brcv functions inside. How do you send data with PCS 7 to an H CPU that has not been configured in the same multiproject? Hope this helps Regards Hosein |
Last edited by: hosein8419 at: 03/08/2021 00:20:56Last edited by: Jen_Moderator at: 03/08/2021 07:20:19Optimized links. |
|
This contribution was helpful to
|
|
Follow us on