(0)| 3/2/2021 1:23 PM | |
|
Posts: 3 Rating:
|
Hello everyone, i would like to use the upload device as new station (hardware and software) feature from tia portal. Does anyone know how I can call this function in opennes? i want to add the configuration of a empty PLC to my project. thank you in advance! Attachment2021-03-02 13_22_51-Siemens - C__Users_Tim Eulink_OneDrive - Graafschap College_Stages en Werk_I@o.png (688 Downloads) |
Last edited by: TimEulink at: 03/02/2021 13:26:22 |
|
| 3/12/2021 2:03 PM | |
|
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello TimEulink, you can upload a station into a project through StationUploadProvider (accessed from a given project). But the upload into a DeviceGroup is not supported. If you use the project to execute an upload, an instance of StationUploadProvider will be returned on GetService call, else the service will return null. See also the information in the manual: Uploading hardware, software and files to PLC device With best regards |
Follow us on