4/12/2008 12:09 AM | |
Posts: 2661 Rating: (279) |
You can find this by checking the performance data of the CPU. Click on the CPU, then PLC, then Module Information and then on the Performance Data tab. See attached screenshot. Please note that you can access the performance data only when you are online with CPU. Alternately you can look-up in the manual. See link below: S7-300 Instruction List CPU 31xC, CPU 31x, IM 151-7 CPU, IM 154-8 CPU, BM 147-1 CPU, BM 147-2 CPU: http://support.automation.siemens.com/WW/view/en/13206730 AttachmentDokument1.pdf (427 Downloads) |
Follow us on