3/20/2019 4:23 PM | |
Joined: 6/4/2010 Last visit: 7/29/2024 Posts: 386 Rating:
|
Dear forum member,
You can do both in the Desigo CC Graphic.
Requirement 1: Sum up the analog values It’s possible by using the standard graphic script in the expression of text symbols. Please find attached to this thread a word file with several possible graphic script expressions which can be used.
Requirement 2: Change the font color of analog values if they exceed or decreed a certain limit You can fulfill this requirement by using the Evaluation Editor expression in the symbol. Such kind of options are trained in the Desigo CC Graphic training course.
You can find some information about how this can be done in the document attached to this thread.
Best regards, Albis AttachmentExamplesScriptReadPX_Color.docx (691 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on