1/20/2021 10:49 AM | |
Joined: 9/23/2005 Last visit: 6/7/2024 Posts: 4341 Rating: (1430)
|
Hi, Sometimes it is not possible to perform a configuration download (for example, when the target device is not physically connected to the engineering station). In this situation the configuration could be transferred as archive (by e-mail, USB stick, etc.) and loaded on the runtime system. It is called as offline project transfer or transfer by archive. Main steps: On the engineering station:
On the runtime station
On the HMI
More details in the HMI manual at HMI Comfort V18 Operating instructions |
Last edited by: Denilson Pegaia at: 09/21/2023 17:34:51Last edited by: Denilson Pegaia at: 09/21/2023 17:35:12Denilson Pegaia |
|
This contribution was helpful to5 thankful Users |
Follow us on