1/16/2013 6:09 PM | ||||||||||||||||||
Joined: 1/28/2009 Last visit: 7/15/2024 Posts: 6844 Rating: (1364)
|
Hello, Check this sample: DP link between CPU 315-2DP (slave) and S7-400 (master) with STEP 7 V5.3
Finally also check the concise description(DP I-Slave modules LADDR.jpg ) by our well-experienced expert in Communication and Networks "fritz". Best regards Hamid Hosseini |
|||||||||||||||||
Last edited by: hdhosseini at: 1/16/2013 6:16 PM |
||||||||||||||||||
This contribution was helpful to1 thankful Users |
1/17/2013 7:18 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (714)
|
Hello, You should allso have a look at the Training modules. D6 - PROFIBUS DP with Master CPU 315-2 DP / Slave CPU 315-2DPAnd more usefull documents with example projects. Regards, Marcjan |
Problem solved? |
|
1/17/2013 5:58 PM | |
Posts: 23 Rating: (0) |
Thank s friend s. All information can help me to finish my project Best regards George |
This contribution was helpful to2 thankful Users |
1/20/2013 4:49 PM | |
Posts: 23 Rating: (0) |
Hi Hosseini. I made a simple sample program for 2 plc s cpu 300 and i need your opinion about sample attach. I need to exchange data beetwen master and slave and I'm sure i made mistakes because it s not working in plcsim.Can u help me and change a sample (in LAD language) to be okay? Thank s Best regards George
Attachment2plcpr~1.zip (377 Downloads) |
1/24/2013 10:41 AM | |
Joined: 1/28/2009 Last visit: 7/15/2024 Posts: 6844 Rating: (1364) |
Dear ChessMaster,
You mean ,for example, to trigger input signals in Master side instead of triggering output signal in slave side.That is possible but does not look natural .Also, I am not sure you can use simulator for SFC14, SFC15 as it may generate error(808x-->System error with external DP interface module).
There is other options when using CPs for PROFIBUS that support for example FDL, S7 Connection.It is possible to simulate communication between 2 CPUs with S7 connection with some system function blocks. check it here: How do you simulate communication between two CPU modules?
Best regards Hamid Hosseini |
Follow us on