7/26/2011 6:11 PM | |
Posts: 2661 Rating: (279)
|
You mean you do not have the PCS7 V7.1 Data Medium Package (software)? Without that you cannot upgrade! |
This contribution was helpful to1 thankful Users |
7/27/2011 6:28 AM | |
Posts: 7 Rating: (0) |
Hello! Special thanks from Phantom75. I have : 1-full package & License of PCS7 V6.1. 2-The DVD of PCS7 V7.1 without License. 3-SIMATIC PCS 7, SOFTWARE, UPGRADE PACKAGE ENGINEERING (AS/OS: PO 250 TO 2000) FROM V6.X TO V7.1 FLOATING LICENSE-(6ES7651-5AC17-0YE5). Please Help me STEP by STEP about the Upgrading of PCS7 from V6.1 to V7.1. Thank you... |
7/27/2011 7:18 AM | |
Posts: 2661 Rating: (279)
|
You seem to have all the required material for the upgrade. See the chapter on installing PCS7 in the following manuals for step-by-step instructions and checklist of requirements: Software update without utilization of new functions (PCS 7 V6.x or higher to V7.1) Software update with utilization of new functions (PCS 7 V6.x or higher to V7.1) |
7/28/2011 5:45 PM | |
Posts: 7 Rating: (0) |
Dear Phantom75 I think occurred a mistake. I've already read this manual.I think these manuals explain the way of upgrading a project to V 7.1. But my problem is ,in the beginning of this way, how i should upgrade my PCS7 from V6.1 to V7.1 ? and then,i want to create a new project in the upgraded PCS7 V7.1. for this reason, First;I should upgrade my PCS7 from Version 6.1 to V7.1. Second;I should create new project in the upgraded PCS7 V7.1.
A)I have Installed PCS7 V6.1. B)I have Installed the original License of PCS7 V6.1. C)I updated my V6.1 PCS7, to V7.1 , by installing the PCS7 V7.1 DVD with selecting the UPDATE Package item.(Please see the attachment.) D)I have Installed the original License for upgrading (V6.x to V7.1) by use of (6ES7651-5AC17-0YE5) package. But after finish this steps, I have the License Error for opening the PCS7 V7.1.
|
7/28/2011 7:14 PM | |
Posts: 2661 Rating: (279)
|
After step D open the ALM (Automation License Manager) click on an old license (V6.x) and then open License Key menu item on top and then click on Upgrade. |
7/29/2011 8:39 AM | |
Posts: 86 Rating: (7) |
SIMATIC PCS 7, SOFTWARE, UPGRADE PACKAGE ENGINEERING (AS/OS: PO 250 TO 2000) FROM V6.X TO V7.1 FLOATING LICENSE-(6ES7651-5AC17-0YE5). What about the part 250 - 2000? do you need also an upgrade for the part licence 250 PO? Yer |
7/30/2011 8:27 AM | |
Posts: 7 Rating: (0) |
Hi! Dear phantom75 Dear Phantom75 ! Dear Yer !
C)During go to Runtime mode for WinCC, Please see the attachment NO.3 for track the D)Also please see the detail about the error in attachment NO.4 in the All Attachments.pdf file. E)After Press "Open" key , please see the attachment NO.5 in the All Attachments.pdf file. After review, I wonder if you could tell me how to solve this problem. Best regards Thak you. AttachmentAll Attachments.pdf (383 Downloads) |
8/2/2011 12:37 AM | |
Posts: 2661 Rating: (279)
|
The license error is normal on the ES. From PCS V7.0 onwards with RC license you can operateruntime only in demo mode (for limited time). If you want to operate runtime on ES indefinitely you need a "special" RT license (not the OS client RT license). |
8/2/2011 2:11 PM | |
Posts: 7 Rating: (0) |
About the RT License,exactly,I will install it. But my question is: I have installed the WinCC RC PO (2000) License, but why the License error occured at WinCC RC PO (2000) ?!!! Another time ,attention to All Attachments.pdf and clarify the answer for me please. AttachmentAll Attachments.pdf (271 Downloads) |
Last edited by: seyed at: 8/2/2011 3:09 PM |
|
Follow us on