8/19/2013 8:06 AM | |
Joined: 4/19/2008 Last visit: 5/21/2024 Posts: 1525 Rating: (159) |
Hello Carlos, Which Version of the Step 7 You have Prviously Installed. Installation requirements:
also If you wish to change to a new operating system, please bear the following in mind:
Service Pack 3 for STEP 7 V5.5 and STEP 7 Professional 2010 |
Ammy |
|
8/19/2013 6:50 PM | |
Posts: 18 Rating: (0) |
Hi, I'm working on WinXP SP3 Pro 32 bits installed on a Virtual Machine (VirtualBox) which it's running on a Linux Mint platform, hardware is AMD FX-4100 Quad Core Processor, Ram assigned to Virtual Machine (WinXP) is 3 GB. My step 7 is Version 5.5 + SP2 and it's working perfectly. |
12/21/2023 12:25 PM | |
Joined: 11/3/2021 Last visit: 5/3/2024 Posts: 1 Rating: (0) |
I have the same issue. can you provide the script please? thanks in advance |
Follow us on