7/26/2013 9:06 PM | |
Posts: 8946 Rating:
|
hello friends, does any one already have done a function to controll ABB Inverter ACS880 with DP - Modul FPBA-01, ProfiDrive profile? Thanks! |
7/27/2013 11:01 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
ACS800=!ACS880 With ACS880 the DriveMonitor is actuallyhttp://www.abb.com/product/seitp322/5a2 ... 4e228.aspx(Drive Composer). (The old software is called DriveMonitor which is valid for ACS800, ACS600, ACS450..).(It is possible to migrate the parameters from ACS800 to ACS880). And, of course like all new software you can use USB connection between drive and PC. FO connection cable with PCMCIA card is not useful in case of ACS880. In case of ACS800 that kind of connection is OK. To give you more info about application - it is keeping the water lavel in limits. There a tank with two pumps which are controled by two ACS880. According to the level there is changing the reference speed. (One pump is working, the other is on stanby). Until now there are no serious problems with drives. According to me the new ACS880 drives are more sensitive to the input power supply line. Best regards, Hristo Mihalev |
This contribution was helpful to
2 thankful Users |
7/28/2013 5:03 AM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating:
|
Dear UMENCHO RMIO is same or different? if it is same, cant we use FO? because in ACS800, we are connecting PCI card to RMIO using FO, some DDCS communication Node 3 Can we use this new software in ACS 800? Is it free or licensed? |
Last edited by: Vithani at: 7/28/2013 5:10 AMI dont Like people driving Fast, thats the reason I overtake them ;) |
|
7/28/2013 8:31 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
Like in other software Pro version of Drive Composer is licensed. ACS880 is a new generation of ABB drive. And the hardware there is completely different. Even in dimensions the new ACS880 is very compact, at least two times smaller. The new software is not possible to use with ACS800 the meaning of online connection with drives. But backup file of ACS800 is possible to 'migrate' there. Finel confirmation on Monday. Best regards, Hristo Mihalev
|
This contribution was helpful to
2 thankful Users |
Follow us on