6/7/2016 4:06 AM | |
Joined: 11/23/2012 Last visit: 10/20/2020 Posts: 6 Rating: (0) |
Hi I am having the same problem in locating the HSP for SM1231. The link https://support.industry.siemens.com/cs/attachments/72341852/TIA_Portal_V11_HSP.zip does not seem to list the HSP for 231-5QD32-0XB0, which is the hardware Input module I'm using. Am I missing something? Has it been missed in the list of files? I am using TIA 11 SP2. Attached is the list of HSP's I can access. I have added HSP's using the File search button. I cannot get my PLC to go to 'RUN' as it shows an error and the LED's are flashing. I cannot perform a "change Device" from the current HW number which is 231-5QD30-0XB0 as there is no correct HSC to select. I have managed to update other hardware such as for 222-1HH32-0XB0. I also just realised I cannot find a Device in the list of CPU's for the s7-1217C PLC I am trying to fit to the machine as I want to user it's faster encoder input capability. The current CPU is a 1214C. Please answer soon if possible as I'm stuck! ------------------------------------------------------------------------------------------ |
Last edited by: mods315 at: 6/7/2016 7:15:12 AMLast edited by: The Helping Hand at: 6/7/2016 9:04:50 AMNew subject after splitting |
|
6/7/2016 9:42 AM | |
Joined: 4/24/2006 Last visit: 6/5/2024 Posts: 8672 Rating: (1158) |
Hello mods315, You will have to upgrade your TIA Portal software. Have a look at the following link: Sales/Delivery Release of the innovated S7-1200 Signal and Communication Modules Sales/Delivery Release: S7-1200 CPU V4.0, CPU 1217C and IO-Link Master SM 1278 Best regards, Wizard |